Overview: Detect Inactivity

Use this operation to detect fields that have become inactive. Inactive fields are identified when the values don’t change for a specified period - this period can be either timestamp or row based. This operation will then mark the values that fall outside the period as bad quality and will assign a null value.

To use this operation effectively, you need in-depth knowledge of the process and the limits of inactivity that are acceptable.

Properties

Category:

Modify

Performance risk:

High potential performance risk. The performance is influenced by the size of the text file being imported, which is determined by number of rows and/or the number of columns of the dataset.

Knowledge required:

Working knowledge of the software.

 

Effect on datasets

How many datasets are required to perform this operation?

One

Does it create a new dataset?

No

Can you reconfigure this operation?

Yes

Can you apply this operation to a locked dataset?

No

Does it modify the current dataset in any way?

Yes

Requirements

  • For row based inactivity detection, a row number column is required.

  • For time based inactivity detection, a timestamp column is required.

Results

  • Values which are considered inactive will be replaced by NULL and will thus be deemed as bad quality.

  • The null values will be created PER FIELD, not across rows and therefore affecting all fields.


Related topics:

  

CSense 2023- Last updated: June 24,2025